Authorized Distributor ofKEY-BAK

KEY-BAK

KEY-BAK's catalogue includes heavy-duty / lightweight retractable keychains, ID badge & access card retractors, tool tethers, industrial machinery reels and accessories. The brand's retractable keychains have a black polycarbonate case for impact resistance and a retractable cord made from DuPont Kevlar fibre for enhanced durability and ruggedness. These heavy-duty keychains' oversized split ring allows attaching of large number of keys & small tools. They can then be secured / clipped on a user's belt. When required, users can just pull the keys out and let them go when the work is done. Selected models come with a nylon key silencer case that wraps completely around and closes with a hook & loop to secure the keys. Their large flaps keep keys silent to prevent unwanted noise and theft.

See More

Request a Quote

KEY-BAK Key Rings

Key Rings (74 Products) Used to carry and secure retractable ID cards in hospitals, clinics and other medical facilities. These key rings offer circular steel rings, key reels with kevlar cords and more.

KEY-BAK Key Accessories

Key Accessories (124 Products) Offer efficient solutions for carrying & organizing keys. Available in snap-on carabiners, pro-case & more options. For those who need to carry multiple keys, a clip-on key rack with multiple carabiners in assorted colours can be useful for quick and easy identification of the required key.

Things To Consider

Cross-Reference Alternatives

KEY-BAK MPNs cross individual references to the equivalent Battalion, Brady and Lucky Line Products. So, if you're looking for a competitor item that is either out of stock or obsolete, chances are Raptor Supplies has the equivalent KEY-BAK products available.

Shipping

These KEY-BAK products range from small to large sizes. They may require careful packaging as some items might get damaged while shipping. Hence, these items are delivered by courier shipment and air freight for minimum downtime.

About KEY-BAK

KEY-BAK's catalogue includes heavy-duty / lightweight retractable keychains, ID badge & access card retractors, tool tethers, industrial machinery reels and accessories. The brand's retractable keychains have a black polycarbonate case for impact resistance and a retractable cord made from DuPont Kevlar fibre for enhanced durability and ruggedness. These heavy-duty keychains' oversized split ring allows attaching of large number of keys & small tools. They can then be secured / clipped on a user's belt. When required, users can just pull the keys out and let them go when the work is done. Selected models come with a nylon key silencer case that wraps completely around and closes with a hook & loop to secure the keys. Their large flaps keep keys silent to prevent unwanted noise and theft.

Major Trade Names

SIDEKICK Series Key Reels

SIDEKICK Series Key Reels

These units feature split-ring and vinyl strap end attachments to securely hold up to 5 office keys and identification cards for easy access. They include heavy-duty Kevlar cord and durable polycarbonate case for use in harsh conditions. These key reels are available with a lightweight zinc alloy ca ... rabiner or paracord lanyard with a spring-loaded cinch for quick attachment with the pocket or belt.

RATCH-IT Key Reels

RATCH-IT Key Reels

These reels feature a built-in ratchet mechanism that locks the reel in 5 inches intervals to remove tension while using the key reels. To unlock the reel, users can simply tug on the cord and retract it. They are available with black carabiners and belt clip attachment options.

MINI-BAK Series Retracting Reels

MINI-BAK Series Retracting Reels

These units are suitable for keeping keys, ID badges, pens and small tools accessible and ready for everyday use. They feature a nylon cord ensuring impact resistance and have a maximum reach of 36 inches and a retraction force of up to 4 ounces. They are available in belt and swivel clip attachment ... styles.

ToolMate Tool Tethers

ToolMate Tool Tethers

These ANSI-certified units are ideal for connecting the tool attachment to the anchor attachment, providing maximum support. They offer minimal retraction force to keep the tethers as short as possible while not making the tool difficult to use. They also help to eliminate snagging or entanglement p ... roblems caused by non-self-retracting tool tethers.

KEY-BAK Competitive Advantages

SUPER48 Ball-Joint Lock

SUPER48 Ball-Joint Lock

The patented ball-joint lock is the main advantage of a retractable heavy-duty key holder that helps to keep the keys secure when not in use. The ball joint point also lets the user exceed the retraction force (which otherwise is limited to the amount of weight specified on other models) and lock the keys when the user does not require them to prev ... ent sagging.

Frequently Asked Questions

Q. What are auto-locking carabiners in a tool tether?

A. Auto-locking carabiners are designed to automatically lock when weight is applied to the spring-loaded gate, making them perfect for applications where the risk of accidental release is high. The user needs to push a small lever or twist the gate to release the lock. Such carabiners are ideal for industries like construction, oil & gas and utilities, providing a quick and secure way to handle tools and prevent them from falling.

Q. What is the advantage of spring-loaded cinch?

A. The spring-loaded cinch provides quick and easy adjustment of the length of the lanyard to fit the needs and then locks in place to offer a secure hold.

Q. How does a retractable ID badge reel work?

A. A retractable ID badge reel features a retractable cord that allows the user to easily extend the ID badge for scanning or inspection and then retract it back into the casing when not in use. This helps to keep the badge secure and within reach, while also preventing it from getting on the way or becoming tangled.