SCOTCH

The company's extensive product line includes tapes, laminators & Vinyls, precision scissors, indoor fasteners, straps & hangers, packaging supplies, strips, clips & covers; dispensers, felt pads, caster cups, chair tips, sliders, chair glides, bumpers and other accessories. Scotch's packaging tapes are designed to securely close a wide variety of heavy-weight boxes and feature a polypropylene film backing with a synthetic rubber adhesive to deliver conformability under stress. They can easily unwind and resist abrasion, moisture and scuffing, hence can be utilised on high-speed automated packaging lines. They also have a high edge tear and split resistance and can withstand temperatures up to 140 degrees Fahrenheit. The brand's tape dispensers come with a pistol-grip design that allows the operator to tack, roll, buff and tear tape in one fluid motion. Their adjustable, hub-mounted brake controls the tension and provides effective sealing along the box seam, preventing waste.

See More

Request a Quote

Things To Consider

Cross-Reference Alternatives

Scotch MPNs cross individual references to the equivalent 3M and Intertape adhesive sealants and tapes. So, if you're looking for a competitor item that is either out of stock or obsolete, chances are Raptor Supplies has the equivalent Scotch products available.

Shipping

These Scotch products range from small to large sizes. They may require careful packaging as some items might get damaged while shipping. Hence, these Scotch items are delivered by courier shipment and air freight for minimum downtime.

About SCOTCH

The company's extensive product line includes tapes, laminators & Vinyls, precision scissors, indoor fasteners, straps & hangers, packaging supplies, strips, clips & covers; dispensers, felt pads, caster cups, chair tips, sliders, chair glides, bumpers and other accessories. Scotch's packaging tapes are designed to securely close a wide variety of heavy-weight boxes and feature a polypropylene film backing with a synthetic rubber adhesive to deliver conformability under stress. They can easily unwind and resist abrasion, moisture and scuffing, hence can be utilised on high-speed automated packaging lines. They also have a high edge tear and split resistance and can withstand temperatures up to 140 degrees Fahrenheit. The brand's tape dispensers come with a pistol-grip design that allows the operator to tack, roll, buff and tear tape in one fluid motion. Their adjustable, hub-mounted brake controls the tension and provides effective sealing along the box seam, preventing waste.

Major Trade Names

Scotch Magic Tape

Scotch Magic Tape

Scotch Magic Tape is an invisible matte-finish tape that provide a strong, secure and permanent seal using 3M adhesive technology. It is ideal for quick fixes and mends original documents or special photos. It uses tape dispensers (included) to let the tape roll out easily and cut evenly with minima ... l wastage.

Scotch-Mount Extreme Double-Sided Mounting Tape

Scotch-Mount Extreme Double-Sided Mounting Tape

This double-sided tape with its 3M industrial strength adhesive, delivers a superior, conformable bond on contact and can hold an item up to 30 lb. It is used on painted drywall, painted / finished wood, metal, Acrylic, smooth stone and painted concrete, providing a smooth & seamless look and elimin ... ating the need for nails and screws.

Scotch Extreme Premium Vinyls

Scotch Extreme Premium Vinyls

These products are designed with proprietary technology by 3M for ultimate precise placement, bubble-free application and conformability. They feature 3M's Comply adhesive with air release channels that easily remove trapped air for a clean, professional finish every time. These premium vinyls are w ... ashable, water-resistant and can withstand temperatures ranging from -40 to 200 degrees Fahrenheit. They never damage a surface or leave residue behind and are compatible with machines like Cricut, Silhouette Cameo and Brother ScanNCut.

Scotch Advanced Thermal Laminator

Scotch Advanced Thermal Laminator

This laminator uses heat to fuse a layer of protective film onto a paper or plastic substrate. It takes up a minute to warm up before application and has an extra wide 13 inch input, making it perfect for both small and big projects. It includes features like a built-in carry handle for portability, ... touch-button controls for user convenience, two heat settings for both 3 mil and 5 mil pouches and dual heated rollers for bubble-free results.

SCOTCH Competitive Advantages

Comply Technology

Comply Technology

The innovative technology has a micro-replicated pattern (multiple air release channels) embossed onto the liner that resembles a 'waffle structure'. These channels allow the air to get extracted and not get trapped between the film and the surface, thus providing a fast, easy and bubble-free installation. This pressure-activated adhesive conforms ... to flat surfaces, simple / compound curves and corrugations, allowing easy sliding, tacking, snapping and repositioning for a seamless application.

Frequently Asked Questions

Q. What is the difference between Scotch Magic tape and transparent tape?

A. Scotch transparent tape has glossy finish, while Scotch Magic tape is frosty on the roll but invisible on paper, making it perfect for writing with a pencil or pen.

Q. Are packaging tapes waterproof / weatherproof?

A. Scotch packaging tapes can withstand a moderate amount of moisture for a short period but are not designed to hold for long & harsh weather conditions.

Q. How to refill a packaging tape dispenser?

A.

  • Remove the old tape core. Place the new roll of tape on the large roller and press down properly. Ensure that the sticky side of the tape is facing down.
  • Gently pull the tape over the guide bar (near the handle) and under the second, smaller roller.
  • Pull the tape against the serrated edge and start taping items.

Q. Does the Scotch laminating machine have any energy-saving features?

A. Selected models of thermal laminators have a built-in auto shut-off feature that turns off automatically after one hour of non-use, thus conserving energy.